How do we have to understand the parameter "maximum overload Voltage +-30VDC" in a the module BMEAH? Does it means +-30VDC in absolute or +-30 VDC in measuring loop 24VDC...?
The customer needs to get a clarification of the parameter „"maximum overload Voltage +-30 VDC" delivered for the module BMEAHI0812. The customer could think that it means +-30VDC in absolute or +-30 VDC in measuring loop 24VDC meaning 24VDC +-30VDC means 24+30 = 54VDC as maximum overload voltage.
The answer is +-30VDC, not +-54VDC.
The answer is +-30VDC, not +-54VDC.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.