Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the IO module be used for ground fault alarm?
Issue:
Can the IO module be used for ground fault alarm with Masterpact and Powerpact breakers?

Product Line:
Circuit Breakers

Environment:
Powerpact P and R, Masterpact NT and NW.  With P and H trip units.

Resolution:
Yes. EcoStruxure Power Commission software version 2.12 released March 29, 2019  has GF alarm functionality through FW update to the IO module. EcoStruxure Power Commission software prior to version 2.12 does not have GF alarm functionality.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: