Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to activate DC injection braking [DC INJECTION]- dCI in ATV71 - ATV61 drive?
Hello,

DC injection braking is activated through below parameters

- Stt [Type of stop] = [DC injection] (dCI): DC injection stop ---> when you apply stop command the DC injection braking is active.

- dCI [DC injection assign.] = LI1 to LIx ---> The DC Breaking is activated when you give this assigned Logic input LIx - When you apply this logic input (if assigned) it will apply DC injection breaking.

Please refer the programming manual extract for the related parameter setting.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV71-ATV61 DC injection Braking.pdf [108.18 KB]