Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 32P - Directional active overpower?
Two-way protection based on calculated active power, for the following applications:
  • active overpower protection to detect overloads and allow load shedding
  • reverse active power protection:
  1. against generators running like motors when the generators consume active power
  2. against motors running like generators when the motors supply active power.