Sometimes, using Windows 10 with Internet Explorer (Version11) or after an update of Windows 10, the Vijeo designer application is not displayed correctly in the Webgate : the project is slided on the left of the screen.
The Webgate is starting correctly but the HMI image is partially displayed.
See below:

This issue could be caused by Win10 scaling feature.
The Win10 supports high DPI display that can scale your desktop from 100% to 150% in display setting.
The Vijeo-designer runtime doesn’t support this setting.
When the runtime runs standalone, it won’t has problem.
But if the runtime runs inside the Internet Explorer, that could be the problem because the latest Internet Explorer is a High DPI supported application, if it changes the DPI setting, our VJD won’t response that. So, the coordinate calculation will be incorrectly.
Our proposal is to not use scale setting in display (set it to 100%) and do not use zoom function in Internet Explorer.
Please use settings as you can see below:
The Webgate is starting correctly but the HMI image is partially displayed.
See below:
This issue could be caused by Win10 scaling feature.
The Win10 supports high DPI display that can scale your desktop from 100% to 150% in display setting.
The Vijeo-designer runtime doesn’t support this setting.
When the runtime runs standalone, it won’t has problem.
But if the runtime runs inside the Internet Explorer, that could be the problem because the latest Internet Explorer is a High DPI supported application, if it changes the DPI setting, our VJD won’t response that. So, the coordinate calculation will be incorrectly.
Our proposal is to not use scale setting in display (set it to 100%) and do not use zoom function in Internet Explorer.
Please use settings as you can see below:
Released for: Schneider Electric Egypt and North East Africa


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.