Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV340 have it's own external keypad?
Issue:
External keypad on the ATV340.

Product Line:
Altivar 340

Environment:
All

Cause:
Part number request

Resolution:
Yes, the ATV340 works with the VW3A1113 external keypad. This remote keypad is not shipped with the ATV340. It must be ordered separately.

https://www.se.com/us/en/product/VW3A1113/plain-text-display-terminal---128-x-64-pixels---ip21/
vw3s1113