Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default IP address for the ION7650 Remote Display (M765RD)

Issue
User needs to connect to the M765RD remote display, but does not now the default IP address

Product Line
M765RD, M765RDPS, S765RD, S765RDPS

Environment
Remote Displays

Cause
The remote displays for the ION7650 meters have a default IP address based on the MAC address of the device

Resolution
To find the default IP address for these remote displays located the MAC address on the label located on the back of the display. After  you have the MAC address follow the steps below.

1.) The format of the IP address is 172.16.nnn.nnn
2.) The last two octets are derived by the last two bytes of the MAC address.
3.) Convert the last 2 bytes from Hexadecimal to Decimal
4.) Insert the two numbers into the format in step 1.

See the example below:
Display MAC address: 00:60:78:01:12:DC

The last 2 bytes are 12 and DC respectively

Hex Conversion of the bytes:
12 = 18
DC = 220


Insert the converted bytes into the format from step 1.
172.16.18.220

Schneider Electric Egypt and North East Africa