Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the NFPA Hazard Rating for Smart-UPS?


Issue:

What is the NFPA Hazard Rating for Smart-UPS?

Product Line:

Smart-UPS

Environment:

All models, All Serial Numbers

Cause:

"NFPA 704: Standard System for the Identification of the Hazards of Materials for Emergency Response" is a standard maintained by the U.S.-based National Fire Protection Association. Some local jurisdictions require this information for all installed equipment

Resolution:

The NFPA Hazard Rating for non-spillable lead acid batteries is based on Sulfuric acid:

Flammability (Red) = 0
Health (Blue) = 3
Reactivity (Yellow) = 2  (Sulfuric acid is water-reactive if concentrated)


img1