This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Protection of motors against voltage sags or detection of abnormally low network voltage to trigger automatic load shedding or source transfer.
Works with phase-to-phase voltage (Sepam series 20 and Sepam series 40) or phase-to-neutral voltage
(Sepam series 40 only), each voltage being monitored separately.
Works with phase-to-phase voltage (Sepam series 20 and Sepam series 40) or phase-to-neutral voltage
(Sepam series 40 only), each voltage being monitored separately.
Released for: Schneider Electric Egypt and North East Africa