This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Control of breaking devices equipped with different types of closing and tripping coils:
conditions.
With Sepam series 20, it is necessary to use an MES114 module in order to have all the required logic inputs.
- circuit breakers with shunt or undervoltage trip coils
- latching contactors with shunt trip coils
- protection functions
- breaking device status data
- remote control orders
- specific control functions for each application (e.g. recloser).
conditions.
With Sepam series 20, it is necessary to use an MES114 module in order to have all the required logic inputs.
Released for: Schneider Electric Egypt and North East Africa