This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The tripping outputs for all the protection functions and all the logic inputs can be
latched individually. The latched information is saved in the event of an auxiliary
power failure.
(The logic outputs cannot be latched.)
All the latched data may be acknowledged:
contactor control function, can be used to create the ANSI 86 “Lockout relay”
function.
latched individually. The latched information is saved in the event of an auxiliary
power failure.
(The logic outputs cannot be latched.)
All the latched data may be acknowledged:
- locally, with the key
- remotely via a logic input
- or via the communication link.
contactor control function, can be used to create the ANSI 86 “Lockout relay”
function.
Released for: Schneider Electric Egypt and North East Africa