Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 87M - Machine differential?
Phase-to-phase short-circuit protection, based on phase by phase comparison of the
currents on motor and generator windings.
Characteristics
  • instantaneous tripping
  • fixed high set point for fast tripping for violent faults, with no restraint
  • percentage-based characteristic with fixed slope and adjustable low set point
  • tripping restraint according to percentage characteristic activated by detection of:
*external fault or machine starting
*sensor saturation or disconnection
*transformer energizing (harmonic 2 restraint)