Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the definition of ANSI 37P - Directional active underpower?
Two-way protection based on calculated active power
Checking of active power flows:
  • to adapt the number of parallel sources to fit the network load power demand
  • to create an isolated system in an installation with its own generating unit.