Issue
In EcoStruxure Machine Expert / SoMachine, is it possible to create a Structure Variable consisting of mixed Persistent and Non-Persistent Variable leaf elements?
For example, we wish to have MyINT and MyWord Non-Persistent and MyBOOL as Persistent below:
DUT Type Definition
TYPE MyStructType :
STRUCT
MyINT : INT;
MyWORD : WORD;
MyBOOL : BOOL;
END_STRUCT
END_TYPE
Structure Variable Definition in Global Variable List (GVL):
VAR_GLOBAL
ThisStruct : MyStructType;
END_VAR
Product Line
SoMachine
EcoStruxure Machine Expert
Environment
PLC Configuration Software
Resolution
No. It is not possible to create a Structure Variable that has leaf-element Variables that consist of mixed Persistent and Non-Persistent Variables.
Fully Persistent Structure Variables must be defined in the PersistentVars object, while Non-Persistent Structures must be defined in either a POU's Variable Definition box or the Global Variable List (GVL) separately.
Example:
The original Structure from the above Example can be split into two Structures defined in the GVL and PersistentVars objects.
DUT Type Definitions
1) Meant for Non-Persistent:
TYPE MyStructType :
TYPE MyStructType :
STRUCT
MyINT : INT;
MyWORD : WORD;
END_STRUCT
END_TYPE
2) Meant for Persistent:
TYPE MyPersistentStructType :
STRUCT
MyBool : BOOL;
END_STRUCT
END_TYPE
Structure Variable Definition in Global Variable List (GVL):
VAR_GLOBAL
NonPersistentStruct : MyStructType;
END_VAR
Structure Variable Definition in PersistentVars:
VAR_GLOBAL PERSISTENT RETAIN
PersistentStruct : MyPersistentStructType
END_VAR
Released for: Schneider Electric Egypt and North East Africa