Issue:
Required control voltage for the ATS48.
Product Line:
Altistart 48 Soft Starter
Environment:
All
Cause:
Installation documentation
Resolution:
ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz
ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz
This is AC voltage, and is applied to the CL1 and CL2 terminals.

Required control voltage for the ATS48.
Product Line:
Altistart 48 Soft Starter
Environment:
All
Cause:
Installation documentation
Resolution:
ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz
ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz
This is AC voltage, and is applied to the CL1 and CL2 terminals.
Released for: Schneider Electric Egypt and North East Africa