Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to export SoMove file for Schneider Electric AC Drive and Soft starter?

Issue:
Is it possible to Export SoMove file for AC Drive and Soft starter.

Product Line:
Altivar AC Drive, Soft starter

Environment:
All

Cause:
Customer wanted to save SoMove file of the ATV320 in PDF file.

Resolution:
In SoMove,
1) Click on File on the Menu Bar
2) Scroll down to Export and select "Export to PDF file"
(Note: Can also Export to .XLS or .TXT file)
3) Create a file name for your PDF file in the Save As Window
4) Click Save to save PDF file in your folder