Issue
PM8000 Series is not communicating with PME 7.2.x, but is communicating with other software applications (e.g., ION Setup, or any Modbus register reader)
Production Line
PM8000 Series
Environment
PM8000 Series Software Updates
Cause
PM8000 might be requiring further support software to be able to communicate with PME 7.2.x
Resolution
Step #1: Make sure that the PM8000 Series meter has the latest firmware version installed.
PM8000 Software and Firmware
Step #2: Download the .zip file in the link below to find the installer file (.exe) which will add support for PM8000 Series in PME 7.2.x
PM8000 Series Device Updater for PME 7.2.x.(ENG)
Released for: Schneider Electric Egypt and North East Africa