Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the list of BIST Error Codes for the ION 7650, ION8650, ION8800, and PM8000 series meters?

Issue
What is the list of BIST Error Codes for the ION7650, ION8650, ION8800, and PM8000 series meters?

Product Line
ION7650
ION8650
ION8800
PM8000

Environment
BIST Error Codes

Cause
What BIST Error corresponds to the Bit value for the DIA1 BIST Status

Resolution
This table will attempt to be a comprehensive list of possible BIST error codes for the platforms that use BIST. These errors also have a corresponding DGD error code, which will show up in the DGD log when a BIST test fails. Refer the BIST section in the DGD Codes.

BIST ErrorDescription7650 Bit8650 Bit8800 BitPM8000 Bit
BIST_DRAMCodeErrorCRC of code image in DRAM has changed0x000000010x000000010x000000010x00000001
BIST_HCycleDeadlineErrorHalf cycle task time exceeded deadline0x000000020x000000020x000000020x00000002
BIST_OneSecondDeadlineErrorOne second task time exceeded deadline0x000000040x000000040x000000040x00000004
BIST_SQRDataErrorSequencer data integrity check failed0x000000080x000000080x000000080x00000008
BIST_DMMDataErrorDMM data failed CRC check0x000000100x000000100x000000100x00000010
BIST_DRAM_SRAMBitTestError0x000000200x000000200x000000200x00000020
BIST_FileSystemThroughputError0x000000400x000000400x00000040
BIST_FlashEraseDeadlineErrorFlash erase time exceeded deadline0x000000800x000000800x000000800x00000080
BIST_AMXCommTaskError0x000001000x000001000x00000100
BIST_HarmonicsTaskDeadlineError0x000002000x000002000x00000200
BIST_FftAggTaskDeadlineError0x000004000x000004000x00000400
BIST_watchdogDeadlineErrorWatchdog tickle deadline was not met0x00000800
BIST_memManageBistWarning0x00001000
BIST_bistTaskDeadlineError0x00002000
BIST_HCycleMarginError0x00004000
BIST_HCycleFpgaSyncError0x00008000