Issue
Where can I download Vijeo Designer v6.2 Service Pack 6?
The version numbers are as follows:
Editor/Buildtime: 6.2.6.39
Runtime: 6.2.6.39
Product Line
Vijeo Designer v6.2
Resolution
Vijeo Designer V6.2 SP6 install files (Updated 2023-02-21) are attached to this FAQ.
1) Just the patch to install on top of the existing Vijeo Designer v6.2 installed on your PC/laptop for the Development Environment (341MB):
"Vijeo_Designer_Development_SP6(6.2.6.39_6.2.6.39).zip"
2) Help files update to your Vijeo Designer v6.2 (Vijeo Designer HTML help files and PDF manuals) - 1129MB:
"SP6_Docs_Pack(6.2.6.39_6.2.6.39).zip"
3) iPC/Standard PC Runtime if you need to have an iPC/Standard PC running as an HMI by itself - 64MB:
"Runtime_For_Windows_SP6(6.2.6.39_6.2.6.39).zip"
4) Data Manager for retrieving Logging/Recipe data from an HMI (this is installed on your laptop/PC on top of your existing Vijeo Designer v6.2) - 61MB:
"DataManager_SP6(6.2.6.39_6.2.6.39).zip"
5) Web Gate Client Files (this is for if you are connecting to the HMI and want to mirror the screen on a remote PC's browser) - 19MB:
"Web_Gate_Client_Files_SP6(6.2.6.39_6.2.6.39).zip"
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa