Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When will the ATV71 become obsolete?
Issue:
ATV71 obsolescence date.

Product Line:
Altivar 71

Environment:
All

Cause:
Date of obsolescence

Resolution:
The ATV71 480V models will become obsolete on January 1, 2020. There is no update yet (as of Jan 1, 2019) on when the other models will be obsoleted.
See attached official letter from the Product Manager.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV71 Obsolescence Date.pdf [1.56 MB]