Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of ACE850TP and ACE850FO network interfaces?
ACE850 multi-protocol communication interfaces are for Sepam series 40 and Sepam series 80 units.
They have two Ethernet communication ports to connect a Sepam unit to a sing
Ethernet network depending on the topology (star or ring):
  • For a star topology, only one communication port is used.
  • For a ring topology, both Ethernet communication ports are used to provide redundancy. This redundancy conforms to the RSTP 802.1d 2004 standard.
Either port can be used for connection:
  • To the S-LAN (Supervisory Local Area Network) port to connect a Sepam unit to
an Ethernet communication network dedicated to supervision, using either of the following protocols:

1- IEC 61850
2- eModbus TCP/IP TRA 15.
  • To the E-LAN (Engineering Local Area Network) port, reserved for remote parameter setting and operation of a Sepam unit using SFT2841 software.
There are two versions of the ACE850 interface, which are identical except for the type of port featured:
  • ACE850TP (Twisted Pair), for connection to an Ethernet network (S-LAN or
E-LAN) using a copper RJ45 10/100 Base TX Ethernet link.
  • ACE850FO (Fiber Optic), for connection to an Ethernet network (S-LAN or E-LAN)
using a 100Base FX fiber optic connection (star or ring).