How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the function of ACE919CA and ACE919CC RS 485 / RS 485 converters?

The ACE919 converters are used to connect a master/central computer equipped
with an RS 485 type serial port as a standard feature to stations connected to a
2-wire RS 485 network.
Without requiring any flow control signals, the ACE919 converters perform network
polarization and impedance matching.
The ACE919 converters also provide a 12 V DC or 24 V DC supply for the distributed
power supply of the Sepam ACE949-2, ACE959 or ACE969 interfaces.
There are 2 types of ACE919 converter:
  • ACE919CC, DC-powered
  • ACE919CA, AC-powered.

Schneider Electric Egypt and North East Africa