Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the main control board for the ATV630 and ATV660 Process drives?
Issue:
Looking for the part number for the Main Control Board for the ATV630 and ATV660 Process drives?

Product Line:
ATV630 and ATV660 Drives

Environment:
All

Cause:
Replacement parts

Resolution:
The MCB or Main Control Board part number for the ATV630 or ATV660 drive is VX4B600100.
Note:  In the US and Canada this part is intended to be installed by Schneider Electric Field Services or their delegates, since it may require special software to be used to ensure it's compatibility with the VFD.
If this is done by someone else, there is no guaranty it will work.
See attached document (which is included in the package with the Control Board) for specific message related to this.

Schneider Electric Egypt and North East Africa

Attachment(s)
EAV64372_00.pdf [146.1 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: