Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset communication on a Serial modbus device when using the Modbus_IOScanner on a Serial_Line in a Modicon M238, M241, M251, M262?

Issue:
How to reset communication on a Serial modbus device when using the Modbus_IOScanner on a Serial_Line in a Modicon M238, M241, M251, M262 PLC?

Product Line:
Modicon M238, M241, M251, M262

Environment:
SoMachine V4.3, EcoStruxure Machine

Resolution:
One can use the ModbusSerialSlave Function block available under the SE_ModbusIOScanner library.
A rising edge to the xReset (BOOL) Input Pin will reset initiate a communication reset.

Depicted below is a representation of the Function Block in EcoStruxure Machine Expert v2.0.2.1:
SE_ModbusIOScanner Library

Schneider Electric Egypt and North East Africa

Attachment(s)
MODBUSIOScanner_reset.jpg [177.19 KB]