Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does my Uni-telway connection fail to connect after installing Vijeo Designer V6.2 SP8?
Issue: The communication between a Magelis HMI and Premium PLC via the Uni-Teleway protocol fails to connect.

Product Line: Vijeo Designer V6.2 SP8 only

Resolution: A software bug in Vijeo Designer V6.2 SP8 caused the Uni-Telway driver to fail to connect a PLC. A hotfix has been released to resolve this issue. Please download the below hotfix.


NOTE: The latest service pack for Vijeo Designer 6.2 is currently SP12. If you would like to upgrade to SP12, please find more information here below:
https://www.se.com/us/en/faqs/FAQ000239885/


Schneider Electric Egypt and North East Africa

Attachment(s)
SP8_Hotfix(6.2.8.2401_6.2.8.2401).zip [343.52 MB]
Web_Gate_Client_Files_SP8_Hotfix(6.2.8.2401_6.2.8.2401).zip [13.16 MB]
Runtime_For_Windows_SP8_Hotfix(6.2.8.2401_6.2.8.2401).zip [60.58 MB]