Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Vijeo Designer Runtime Manager always launches with "Welcome to Vijeo Designer Trial Edition"
Issue: Vijeo Designer Runtime Manager always auto-starts and displays the dialog "Welcome to Vijeo Designer Trial Edition"

Product Line: Vijeo Designer Runtime for iPC/Generic PC

Resolution: This dialog will always appear (even if you have registered the software) when you are running under a user account (ie non-administrator). To stop this message from appearing, you will need to log out of the user account, login as an Administrator and press the "Start/Yes" button on the dialog box "Welcome to Vijeo Designer Trial Edition". This will set a registry key to stop the dialog box from appearing again. Once this is set, you can log back in as the user account. The application will start as expected.