Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV630 - Wants to display the modbus run time on the HMI
Issue:
How to read the Modbus "run time" on a HMI for the Altivar Process Drive.

Product Line:
ATV630, ATV930

Environment:
All serial numbers

Cause:
Wants to display the run time on the HMI

Resolution:
Beginning with ATV630 firmware version 2.4IE11 and ATV930 version 2.1IE17 the keypad can display the Run Time in Days, Hours,Minutes and  Seconds.
When reading the Runtime over a network the value will be in seconds
rtH Parameter name: Total motor operating time Terminal display: [Run time]
Logic address: 3244 = 16#0CAC (unsigned 32 bit)

Previous versions only displayed the run time  in seconds.