Issue:
Suffix N4 and S6 of the ATV320 drive
Product Line:
Altivar ATV320
Environment:
All serial numbers
Cause:
Customer is looking for a replacement for ATV320U22S6, and wanted to know if he can use ATV320U22N4.
Resolution:
The ATV320U22S6 has 575V 3 phase input voltage, and the ATV320U22N4 has 460V 3 phase input voltage. Customer needs to verify the correct 3 phase input voltage to order the correct part number for the ATV320, even though they are the same HP.
Suffix N4 and S6 of the ATV320 drive
Product Line:
Altivar ATV320
Environment:
All serial numbers
Cause:
Customer is looking for a replacement for ATV320U22S6, and wanted to know if he can use ATV320U22N4.
Resolution:
The ATV320U22S6 has 575V 3 phase input voltage, and the ATV320U22N4 has 460V 3 phase input voltage. Customer needs to verify the correct 3 phase input voltage to order the correct part number for the ATV320, even though they are the same HP.
Released for: Schneider Electric Egypt and North East Africa