Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Altivar Process variable speed drive Boosting Motor Voltage for Long Cables?
Yes, there is possibility for overmodulation. Overmodulation increases output voltage up to hexagon form, which means that RMS value as well as fundamental harmonic will increase. Also 3rd harmonic to the motor is generated, but it is not a problem, because motor is 3-phase symetrical and so 3rd harmonic is attenuated in the motor.
Bear in mind that this overmodulation can add only few percents (5-6%) comparing to non-overmodulated (circular form) shape.
See extract page from ATV900 manual. The same is available for ATV600.

Schneider Electric Egypt and North East Africa

Attachment(s)
Extracted pages from ATV900_Programming_Manual_EN_NHA80757_05.pdf [148.62 KB]