Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause a Backlash error [bS9F] fault on an ATV340 series drive?
Issue:
Customer is experiencing a bS9F Backlash error on an ATV340 series drive.

Product Line:
ATV340

Environment:
Backlash Compensation function is being used.

Cause:
The torque threshold used for backlash function can not be reached after [BL Monit Delay] bqt.

Resolution:
 Verify the settings
 Verify the coupling



Schneider Electric Egypt and North East Africa