Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of ACE917 injection adapter?
The ACE917 adapter is used to test the protection chain with a standard injection box, when Sepam is connected to LPCT sensors.

The ACE917 adapter is inserted between:
  • The standard injection box
  • The LPCT test plug:
- integrated in the Sepam CCA670/CCA671 interface connector
- or transferred by means of the CCA613 accessory.

The following are supplied with the ACE917 injection adapter:
  • Power supply cord
  • 3-meter (9.84 ft) cord to connect the ACE917 to the LPCT test plug on CCA670/CCA671 or CCA613.
Characteristics

Power supply: 115/230 V AC
Protection by time-delayed fuse 5 mm x 20 mm (0.2 x 0.79 in ):  0.25 A rating

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center