Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the BMXDAI1614 as a traditional input module if I disable the "Wiring Check" option?
Yes. The BMXDAI1614 will operate as a traditional input when the "Wiring Check" option is turned off.

With this module, you have the ability to monitor each channel separately to determine if a sensor is connected. It does this by monitoring the leakage current of the sensor when it is off. If it detects that no sensor is connected, it will set bit 9 of the CH_FLT.

100766_IMG

Schneider Electric Egypt and North East Africa