Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use the BMXDAI1615 as a traditional input module if I disable the "Wiring Check" option?

Issue:

Can I use the BMXDAI1615 as a traditional input module if I disable the "Wiring Check" option?

Product line:

BMX IO


Resolution:

Yes, the BMXDAI1615 will operate as a traditional input module when the "Wiring Check" option is turned off.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)