Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a difference in the P24 and +24 terminals on the ATV630 drives?
Issue:
Difference between the P24 and +24 terminals on the ATV630 drives.

Product Line:
ATV630

Environment:
All serial numbers

Cause:
N/A

Resolution:
P24 Output power supply for digital inputs and STO  +24 Vdc  Tolerance: –15...+20%  Current: maximum 1.1 A
+24 Digital input power supply   +24 Vdc input supply  Tolerance: –15...+20%  Current: 100 mA

Schneider Electric Egypt and North East Africa