Issue
Where to find the End User License Agreement (EULA) for ION Setup Configuration tool?
Product Line
ION Setup 3.1
ION Setup 3.2
Environment
End User License Agreement (EULA)
Cause
Need a copy of the End User License Agreement (EULA) for the ION Setup Configuration tool to update documentation and information for agency software
Resolution
There are two locations to find the End User License Agreement (EULA) for ION Setup. For where to download the latest version of ION Setup software, refer to FA212816
- Shown during ION Setup Installation
- Can be found in the installer exe. Open up the installer exe using 7-zip, browse the folders (IONSetup v3.2.25092.01 (current version) > ION > setup), and then open the "License.htm" file in Chrome or Internet Explorer
Released for: Schneider Electric Egypt and North East Africa