{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
PowerChute Network Shutdown does not proceed with VM Startup after powering on the vCenter Server VM
Issue:
PowerChute Network Shutdown does not proceed with VM Startup after powering on the vCenter Server VM. PowerChute shows an event log entry “Attempting to start vCenter Server VM <VM Name>” but does not proceed to power on VMs.

Product Line:
PowerChute Network Shutdown v4.2, v4.3, v4.4

Environment:
PowerChute Network Shutdown configured with VMware

Cause:
This can occur when some vCenter Services are unable to start.

Solution:

Connect to the vCenter Server VM and check the status of vCenter Services. Manually start services that have not started.
  • On Windows, the services.msc console can be used.
  • On Linux, execute the following command:
service-control --status -all

Schneider Electric Egypt and North East Africa

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: