Issue:
When a UPS critical event is cleared and PowerChute starts powering on VMs, any prioritized VMs with a 0 second Startup Duration are initially skipped and later powered on.
Product Line:
PowerChute Network Shutdown v4.3, v4.4
Environment:
PowerChute Network Shutdown configured with Nutanix Acropolis Hypervisor (AHV) support
Solution:
This issue will be resolved in the PowerChute Network Shutdown 5.x release.
Alternatively, if your PowerChute configuration includes priority groups with a 0 second Startup Duration, you can disable VM Startup in PowerChute and power on VMs manually following a shutdown.
Released for: Schneider Electric Egypt and North East Africa