Issue:
Programming reference switching and +/- speeds via digital inputs for the ATV630.
Product Line:
Process Drives
Environment:
ATV630 ATV930
Cause:
Setup +/- speed as second reference.
Resolution:
[Complete settings] [Command and Reference]
Freq Switch Assign = Ref Freq Channel 2
Ref Freq 2 Config = Ref Frequency via DI
[Complete settings] [Generic functions] [+/- speed]
[+ Speed Assign] USP = desired DIx Increase speed input assignment.
[- Speed Assign] dSP = desired DIx Down speed input assignment.
Programming reference switching and +/- speeds via digital inputs for the ATV630.
Product Line:
Process Drives
Environment:
ATV630 ATV930
Cause:
Setup +/- speed as second reference.
Resolution:
[Complete settings] [Command and Reference]
Freq Switch Assign = Ref Freq Channel 2
Ref Freq 2 Config = Ref Frequency via DI
[Complete settings] [Generic functions] [+/- speed]
[+ Speed Assign] USP = desired DIx Increase speed input assignment.
[- Speed Assign] dSP = desired DIx Down speed input assignment.
Released for: Schneider Electric Egypt and North East Africa