Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SBO upgrade process failed (SBO 1.8.x to SBO 1.9.x)
Upgrade failed when upgrading Automation Server from SBO version 1.8.x to 1.9.x

Log indicate:
(Device Administrator | View | Last Upgrade Log)
ERROR:        Exception encountered during database upgrade : StartUpMode UpgradeDatabase : RecoverableException: d:\dev\rb-rb-1.9.2-system\source\server\nsp_servers\csc\LonTypes\source\Lon2MapFileUtil.cpp(185) Invalid Data Error: Invalid_Data (0x10000) in module Impex(57). "Map data is too old for type: public.lon2.devicetemplates.pid90003A8200E90401. You need to run the Lon Repair command in the latest version of workstation"
2019-04-10 07:14:02  INFORMATION:  Database upgrade time: 5.28889 seconds
2019-04-10 07:14:02  INFORMATION:  =============  End Configuration Database Upgrade  =============
Source version: 1.8.1.79 Target Version: 1.9.2.45

Stteps
1. Upgrade Workstation and Automation Server to latest available version (SBO 1.8.1.3600)
2. Connect with Workstation to Automation Server
3. Select Server, right click Advanced | Repair LonWorks configuration ...
4. Select Next to repaire when indicated "Server needs to be repaired"
5. Finally upgrade to Version 1.9 using Device Administrator

Schneider Electric Egypt and North East Africa

Attachment(s)
Start repair.PNG.png [120.18 KB]
repair01.PNG.png [37.8 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center