Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Magelis HMI response slowly if the application is using save to file function

1.Issue

Magelis HMI response slowly if the application is using alarm logging/save to file function.
It will take several minutes to come out of screen saver or switch panel after touching the screen.

2.Environment

Issue happens in Magelis HMITargets which is running Vijeo Designer 6.2 SP6 or previous version.

3.Resolution

1.Lower number of records being logged and lower intervals.
2.Upgrade to Vijeo Designer 6.2 SP7 or later and enable “Multiple Subfolders” function(Press “Shift”+”X” in “Save to File” window).
3.Clean USB disk after backing up the data to PC regularly, then plug back the USB disk. It is not for long-term storage of mass data here.

4.FAQ Applicable Conditions

FAQ applies to Basic Panel and Advanced Panel.

Schneider Electric Egypt and North East Africa

Attachment(s)
Save to file.PNG.png [38.24 KB]