Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I find the IP address of an EM4800 after It was changed
Issue:
The end user may have lost the IP address or accidentally changed the IP address for the EM4800 meter

Product Line
EM4800 Series Meter

Environment:
Meter Configuration

Resolution:
You can view the current IP address of the EM4800 by holding the DISPLAY button for 5 seconds. This will activate "Diagnostic Mode". From here you can view the IP address and other nameplate information by toggling the display button down until the IP Address Option is displayed. This is shown the current IP address on the EM4800's display.