Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset pump runtime for each pump involved in booster control?
Pump runtime can be reset by writing zero or can be set to a value written over communication. Pump runtime cannot be reset via SOmove or HMI.
See attached list of addresses for each pump. Writing is possible when the drive is stopped (not in run state). For writing value via modbus or modbus TCP, use logic address. Depending on PLC type you may need to write value to address+1.
Bear in mind that runtime is 32bit value.
For writing the value it is possible to use a free tool like modscan and write value directly from PC

Schneider Electric Egypt and North East Africa

Attachment(s)
Pump runtime parameters.xlsx [9.91 KB]