Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the limitations with the WebTerminal browser HMISTW6 ?
STW6 is a Web HMI that accesses Web servers on an intranet and displays screens. It has the following characteristics.
  • Compatible with an HTML5 server supporting Java Script.
  • Proxy cannot be used.
  • Configure a system of multiple Web HMI units with a daisy chain.

The following features have not been supported yet.
  • Access to Web servers on Internet
  • Access to HTML5 pages on an external storage


Restriction
HMISTW6 is not compatible with the features below.