Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to get PRM Master 1.1.4.0?
Issue
The latest version of PRM 1.2 ISO has the PRM Master DTM is 1.1.3.0, but some projects show the PRM Master DTM as version 1.1.4.0 and the project doesn't build with this discrepancy.

Product Line
Unity Pro, Control Expert, PRM, TCSEGPA23F14F

Environment
Control Expert v14, Unity Pro v13.1

Resolution
On the PRM 1.2 .ISO, you need to launch the index.hta to install a Patch for Master DTM (7-Krohne\MasterDTM\PRMmasterDTMPatch.exe) this patch changes the version of PRM Master from 1.1.3.0 to 1.1.4.0.