Issue
Customer send multiple commands from SCADA within short interval of time ( in ms ). What settings shall be configured in NOR module to accept this commands successfully.
Product Line
BMXNOR0200 V1.7 IR19, WinPP104 ( Licensed Version with customer )
Environment
Windows 10 64 Bit Build 10.1703.1, Control Expert V14.0
Resolution
In the webpage of NOR when configured as server, access the parameter "CMD Queue Size" by Channel > server > session > paramter > Advanced Properties > CMD Queue Size
This CMD Queue size allows us to configure the NOR to accept multiple commands for various datatypes C_SC, C_SO etc in parallel. By default it is zero. User needs to configure
this value to like 10 to perform some test.
Customer send multiple commands from SCADA within short interval of time ( in ms ). What settings shall be configured in NOR module to accept this commands successfully.
Product Line
BMXNOR0200 V1.7 IR19, WinPP104 ( Licensed Version with customer )
Environment
Windows 10 64 Bit Build 10.1703.1, Control Expert V14.0
Resolution
In the webpage of NOR when configured as server, access the parameter "CMD Queue Size" by Channel > server > session > paramter > Advanced Properties > CMD Queue Size
This CMD Queue size allows us to configure the NOR to accept multiple commands for various datatypes C_SC, C_SO etc in parallel. By default it is zero. User needs to configure
this value to like 10 to perform some test.
Released for: Schneider Electric Egypt and North East Africa