How can we help you today?

Is there a limit to the number of POU's in a Control Expert application?

Issue
Is there a limit to the number of POU's (program organization unit)  in a Control Expert application?

Product Line
Control Expert

Environment
Windows 7, Windows 10, Windows 8

Resolution
There is no defined  limit for the maximum number of POU's that a Control Expert or Unity application can have.  The limit is
dependent upon many factors (i.e., application size, available application memory, size of the data structure containing its output
and internal variables defined in the POU's and number of variables configured in the main program of the application, etc.).