Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I configure a BMXDDI1602 module in EcoStruxure Control Expert with a M580 PLC?
Issue
Configure Input Module

Product Line
Modicon x80
Modicon M580

Enviroment
EcoStruxure Control Expert

Resolution
1. Open a M580 Project
2. Open the PLC Bus to see the rack view
3. Add the BMXDDI1602 to the desired slot in the backplane
4. Open the configuration screen for the BMXDDI1602
5. Change the Device DDT name if needed
6. Activate or Deactivate the supply monitoring. This monitors the external 24v supply for the module.
7. Build the project and download to the PLC


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)