Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to implement DC braking in the ATV630?
DC injection braking is activated through below parameters

- Stt [Type of stop] = [DC injection] (dCI): DC injection stop ---> when you apply stop command the DC injection braking is active.
Or
- dCI [DC injection assign.] = LI1 to LIx ---> The DC Breaking is activated when you give this assigned Logic input LIx - When you apply this logic input (if assigned) it will apply DC injection breaking.

In addition to the following:
- IdC [DC inject. level 1] = 0.7 In (range 0.1...1.41 In)
- tdI [DC injection time 1] = 0.5 s (range 0.1...30 s)