Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the IP of GTUX displays?
1.Issue
Notification to customers who are using Schneider-Electric Magelis GTUX Displays
2.Product line
The following displays from GTUX series are concerned by this FAQ: HMIDT35X and HMIDT65X
These displays are used with HMIG3X, HMIG3F0H Boxes
(Note that the Boxes are not directly concerned by the modification of waterproof)
3.Environment

4.Resolution
The specification of waterproof on Schneider-Electric Magelis HMIDT35X, HMIDT65X Displays has been changed depending on the PV version.
If the product version is “PV:01”, the protection level is IP66F.
If the product version is “PV:02” (and greater), the protection level is IP66F, IP67F, Type 4X (indoor and outdoor use), Type 12, Type13.