Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum surface temperature of aluminum PTC heater?
The surface temperature stabilizes at 75°C when the ambient temperature is (-5°C).